Turning harmful use of industrial oil into an asset
Under the brand name, SKF RecondOil, SKF delivers an innovation to turn the environmentally harmful use of industrial oil into an asset that can be used repeatedly with maintained performance. We are making the technology available to customers around the world – both as part of its offer around the rotating shaft, as well as via licensed partners in selected markets.
Molecular Oil Technology is licensed to operate with a RecondOil Double Separation Technology (DST) stand-alone unit from SKF. The DST system removes particulates from industrial oil, allowing it to be regenerated rather than replaced. This will improve the environmental performance and reduce costs for industrial end-users in Mexico.